You are here: Using the PDMM or PCMM Controller > Booting the PDMM or PCMM />

Booting the PDMM or PCMM

This topic explains the boot sequence for the controller, which is based on the RAM and the Flash memory.

The flash memory contains two images:

Boot Sequence

State Display Description
Hardware power on Controller option card has power
Stage 0 Reached after the I2C is initialized
Stage 1 Reached after the DDR3 ram memory is initialized
Stage 2 Reached just after the RAM memory relocation
At this point the boot is running in DDR3 RAM memory
Stage 3 Reached after the flash memory is initialized
Boot Startup Script After all the previous steps, the startup script starts automatically.
QNX startup Reached after the Boot startup script is finished
Sysinit Reached after specific configuration parameters of the target are loaded, and after the network is started using the rotary switch.

When the controller is booted with a cable attached the configured IP address (depending upon the current position of the rotary switch) will be displayed in the 7-segment display (see Display the IP Address of a PDMM or PCMM). If the controller is started without a network connection then the IP address will not be displayed.

After the boot sequence is successful, the controller will be in one of two modes:

Normal operation
Recovery Mode (if firmware download is permitted)

 

Boot Startup Script

Booting from the Recovery Image


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™